Căutare

Conținut principal

  • Înscriere
  • Intrare în cont

Soluţii

Print page

Soluţii

Sisteme de producţie şi distribuţie

Getting material from the receiving docks to the shipping docks as quickly as possible with the least amount of errors is critical to any organization’s success. This takes high level logistical coordination and error-proofing of repetitive processes. Many automation providers allow for the movement of data from one machine to another on the shop floor. However, moving accurate and detailed data from the shop floor up to IT systems has been overlooked by most, resulting in costly down time, process inefficiencies and many other issues.

Getting material from the receiving docks to the shipping docks as quickly as possible with the least amount of errors is critical to any organization’s success. This takes high level logistical coordination and error-proofing of repetitive processes. Many automation providers allow for the movement of data from one machine to another on the shop floor. However, moving accurate and detailed data from the shop floor up to IT systems has been overlooked by most, resulting in costly down time, process inefficiencies and many other issues.

With Mitsubishi Electric’s e-F@ctory solution, these problems have been eradicated. It can provide a true total solution architecture, not only concentrating on the shop floor but also providing a direct interface to ERP/MES systems with streamlined real-time data, resulting in a “visible” system solution.

With so many products and articles being handled in current material handling processes, providing a complete automation platform is paramount to a successful application. With its iQ Platform Mitsubishi Electric provides a single centralized automation platform that easily interfaces with bar code readers, pick/place robots, conveyors, weighing machines, scanners and more. The CC-Link device level network provides a high speed method to integrate such devices easily and at a low cost. Even robots and conveyors can be controlled directly from the controller platform, along with interfaces to the GOT1000 HMI series for real time online control and monitoring. With all of this cohesiveness, the right product being delivered to the right destination is ensured.

Sus